Creating a Copy of a Function or Program
When creating a new function or program, you might find it easier to start with a copy of the current one. The copy that you create is not locked, even if the original is locked.
1. | From the Actions menu, click Create Copy. |
2. | Type a new name, or click OK to accept the proposed name. |
3. | If you want to change the access level, select Library Access, and select a new level. |